Material Safety Data Sheet

Infosafe No™. K1H43 Issue Date: December 2010 ISSUED by SEPTONE CS: 1.4.95
Product Name: WASHROOM HAND SOAP

Not classified as hazardous according to criteria of NOHSC

   
   
         
         
         
   
   
   
   

1. IDENTIFICATION OF THE MATERIAL AND SUPPLIER

Product Name WASHROOM HAND SOAP
Company Name Septone Products Pty Ltd (ABN 50 009 745 537)
Address 44 Aquarium Avenue HEMMANT
QLD 4174
Emergency Tel. After hours only: (07) 3821 0623
Telephone/Fax
Number
Tel: (07) 3390 5044
Fax: (07) 3390 5041
Email general@septone.com.au
Recommended Use Liquid washroom hand soap.
Other Names Name Mancode
MICROWASH IHM5, IHM20
PROTECTA WASH IHPW500, IHPW4L, IHPW5, IHPW20
Other Information The information herein is, to the best of our knowledge, correct and complete. It describes the safety requirements for this product and should not be construed as guaranteeing specific properties. Since methods and conditions of application are beyond our control, Septone does not accept liability for any damages resulting from the use of, or reliance on, this information, in inappropriate contexts.

2. HAZARDS IDENTIFICATION

Hazard
Classification
Not classified as hazardous according to criteria of NOHSC
NON-HAZARDOUS SUBSTANCE.
NON-DANGEROUS GOODS.
Hazard classification according to the criteria of NOHSC.
Dangerous goods classification according to the Australia Dangerous Goods Code.
Risk Phrase(s) Not classified as hazardous according to criteria of NOHSC
Sensitization of
Product
None of the components of this product is considered to be a skin or respiratory sensitiser.
Teratogenicity None of the components of this product is considered to be a teratogen.

3. COMPOSITION/INFORMATION ON INGREDIENTS

Chemical
Characterization
Liquid
Ingredients Name CAS Proportion Hazard R Phrase
Water 7732-18-5 60-100 %
Ingredients determined not to be hazardous - 10-30 % R48

4. FIRST AID MEASURES

Inhalation Remove the victim from the source of exposure. If the victim is not breathing, apply artificial resuscitation.
Ingestion Do NOT induce vomiting. Give water to drink. Seek medical attention.
Skin Remove contaminated clothing and launder before re-use. Wash affected skin with water.
Eye Hold the eyes open and flush with water for at least 15 minutes. Seek medical attention.
First Aid
Facilities
This Material Safety Data Sheet should be provided to the attending medical doctor. Normal washroom facilities are generally suitable. It is recommended that an eyewash station be available and ready for use.
Advice to Doctor Treat symptomatically.

5. FIRE FIGHTING MEASURES

Fire Fighting
Measures
This product is not flammable under the conditions of storage and use and does not support combustion.
Suitable
Extinguishing
Media
Use the extinguisher appropriate to the principal fire hazard or to the source of the fire.
Hazards from
Combustion
Products
If this product is involved in a fire, the water contained in it may evaporate, leaving a residue which may combust. During combustion, the residue may produce carbon monoxide as well as other unidentifiable organic compounds.
Special
Protective
Equipment for
fire fighters
Firefighters are to wear protective equipment appropriate to the principal fire hazard or the source of the fire. No special protective equipment required if this product is involved in a fire.
Specific Hazards None known.

6. ACCIDENTAL RELEASE MEASURES

Spills & Disposal Note: spillages are slippery. Wear appropriate protective equipment. Cordon off the spillage area. Isolate the source of the spillage or leak. Contain the spillage using a suitable non-flammable absorbent material such as sand or diatomaceous earth, and then transfer into sealed plastic containers for disposal.

7. HANDLING AND STORAGE

Handling and
Storage
Store in plastic containers in a clean, dry, cool, well ventilated place away from foodstuffs. Keep containers sealed when not in use. It is recommended that this product be dispensed through approved dispensers.

8. EXPOSURE CONTROLS/PERSONAL PROTECTION

National Exposure
Standards
No value assigned by NOHSC for any ingredients used in this product.
Engineering
Controls
Natural ventilation adequate under normal conditions of use. Keep containers closed when not in use.
Personal
Protective
Equipment
Not required under normal conditions of use. Wear chemical goggles if handling large amounts and if splashing is likely to occur.

9. PHYSICAL AND CHEMICAL PROPERTIES

Form Liquid
Appearance Viscous pearlescent pink liquid. Microwash is unfragranced, Protecta Wash contains a pleasant soapy fragrance.
Boiling Point 100°C
Solubility in
Water
Complete
Specific Gravity 1.015 @ 25°C
pH Value 5.5
Evaporation Rate As for Water
Volatile Component 85% w/v
Flash Point This product will not flash and does not support combustion.
Flammability This product is not flammable under the conditions of use and does not support combustion.

10. STABILITY AND REACTIVITY

Chemical Stability Considered stable. For extended storage life, store below 30°C and keep out of direct sunlight.
Conditions to
Avoid
No known conditions to avoid.
Incompatible
Materials
Strong oxidising agents.
Hazardous
Polymerization
Will not occur.

11. TOXICOLOGICAL INFORMATION

Inhalation Does not present an inhalation hazard.
Ingestion Mild irritant.
Skin Essentially non irritating.
Eye Mild eye irritant.
Chronic Effects No known chronic effects.
Reproductive
Toxicity
None of the components of this product is considered to be toxic to the unborn foetus.
Mutagenicity None of the components of this product is considered to be a mutagen.
Carcinogenicity None of the components of this product is considered to be a carcinogen.

12. ECOLOGICAL INFORMATION

Short Summary of
Assessment of
Environmental
Impact
At normal use levels and following standard effluent treatment, this product is expected to exhibit low toxicity towards aquatic organisms. However, the undiluted material should be prevented from entering waterways. The surfactants used in this product are readily biodegradable when tested according to AS1792-1976. None of the components of this product are expected to bioccumulate.

13. DISPOSAL CONSIDERATIONS

Waste Disposal Dispose of large amounts in a chemical dump according to local authority statutory requirements. For small amounts, wash the product to the drain with a large excess of water.
Container Disposal Empty containers are recyclable.

14. TRANSPORT INFORMATION

Transport
Information
This product is classified as non dangerous according to the ACTDG and according to the IMDG Code.
IMO Marine
Pollutant
None of the components of this product is considered by IMO to be a Marine Pollutant.

15. REGULATORY INFORMATION

Poisons Schedule Not Scheduled
AICS (Australia) To the manufacturer's best knowledge, all components of this product are listed on AICS.

16. OTHER INFORMATION

Contact
Person/Point
Technical Manager (07) 3390 5044

...End Of MSDS...


(C) Copyright ACOHS Pty Ltd
Copyright in the source code of the HTML, PDF, XML, XFO and any other electronic files rendered by an Infosafe system for Infosafe MSDS displayed is the intellectual property of Acohs Pty Ltd.
Copyright in the layout, presentation and appearance of each Infosafe MSDS displayed is the intellectual property of Acohs Pty Ltd.
The compilation of MSDS's displayed is the intellectual property of Acohs Pty Ltd.
Copying of any MSDS displayed is permitted for personal use only and otherwise is not permitted. In particular the MSDS's displayed cannot be copied for the purpose of sale or licence or for inclusion as part of a collection of MSDS without the express written consent of Acohs Pty Ltd.